2 Answers
    Jul 5, 2016 17:30:25 GMT 5.5

    Dear Team

    As I created solution no. ISX0001364253-0005 I found out that the software support-SKU for StruxureWare DCE basic (server software & node licences) does not appear at the relevant bill of material. So I had to add it at manual way.

    Recently this SKU "WMS1YRBASIC" always was a part of relevant BOMS. As I (pretty unfortunately) did not create too much solutions including a DCIM environment, I wonder if there might be a bug in the relevant ISX designer software.
    Could you perhaps take a look at this topic and let me know afterwards, please?
    It would be very kind of you.

    Warmest regards from Southern Germany,
    Uta

    Jul 11, 2016 13:05:19 GMT 5.5

    Hi Uta
    I can not replicate the error. I tried 2 solutions and always got the WMS1YRBASIC, lets hope that was just a minor bug taht is already fixed.

    Jul 11, 2016 13:32:35 GMT 5.5

    Hi Uta,

    We have done the investigation with all the possible test scenarios and we are always getting WMS1YRBASIC in BOM.
    Can you please send us steps to reproduce and all also let us know which version of ISX designer you are using?