1 Answers
    Oct 4, 2017 12:08:19 GMT 5.5

    Hi,

    Under the "Management" tab, we have the options to set up DCE, DCO, etc.
    How are the amount of SKUs (e.g. WNSC010104, WNSC010105...) calculated based on the installed hardware ?

    Currently it is like a black box that just output the final results. Is there anyway for us to know the internal workings? Thank you.

    Oct 11, 2017 12:16:48 GMT 5.5

    Hi Ting,

    I can certainly help you with this. These are SE internal calculations. I will drop you an email with details.

    Best,
    Ravi.