2 Answers
    Feb 23, 2018 6:10:01 GMT 5.5

    Hi,

    Is it possible to add the dialog box when exiting the designer to "Save, Don't Save, and Cancel", rather than just "Save and Cancel"? As it stands right now, the Cancel button is equivalent to a "Don't Save" function, and exits the designer rather than just closing the dialog box. Most programs the cancel button just closes the dialog box and lets you keep working.

    isxdialog.jpg


    Feb 26, 2018 12:14:47 GMT 5.5

    Hi Tim,

    On right top corner of dialog there is red color close button. You can close dialog if you don't want to save/cancel and close the designer.

    Best,
    Ravi.

    Mar 1, 2018 0:45:22 GMT 5.5

    Hi Ravi,

    The red X on the close dialog window acts as a "Close and don't save" button, which is the same action that the "Cancel" button currently performs.

    I am asking for the Cancel button to close the dialog window but keep the designer open. If I accidentally press the exit button in the designer, my only options are to "Save and Exit", or "Don't save and Exit".

    The attached picture shows a typical dialog box for MS Word which explains what I am requesting.

    Thank you

    msworddialog.jpg