4 Answers
    Feb 26, 2018 21:20:44 GMT 5.5

    With Designer open, any time I select a new category to configure, the pop up box that opens is much too small for the amount of content it holds.  I have to manually increase the size of every box after it opens so that I can then make my selections.  It sounds like a small inconvenience, however, over the course of a large solution I could be doing this dozens of times.  That is a lot of time lost.  Also, the font sizes should be increased as well.  For some reason they are very small now and hard to see.  

    Mar 8, 2018 11:29:09 GMT 5.5

    Hi Tim,

    We are really sorry for the inconvenience caused. Please help me with below information to assist you better.

    1. Resolution of you laptop.
    2. Few screen shot showing error.

    Looking forward to hear from you.

    Best,
    Ravi,

    Mar 8, 2018 21:44:23 GMT 5.5

    Hello and thanks for your response. I've increased the display size of text, apps, etc on my 2nd screen which has helped some. However, the size displayed when opening a detailed quote or CTO report is still too small. Would like to have the option in Designer to increase text size if need be. Where can I send print screens for reference?

    Mar 9, 2018 13:29:58 GMT 5.5

    You can send screen shots to [email protected]

    Mar 13, 2018 15:18:51 GMT 5.5

    Hi Tim,

    Waiting for your screen shots..

    Best,
    Ravi.