2 Answers
    Mar 12, 2018 20:06:14 GMT 5.5

    I would like to create a 300 kVA PMM with 3 output panels in Designer. This is no longer possible. Reference ISX0001510172-0006.

    Mar 13, 2018 17:49:35 GMT 5.5

    John
    You will need to do the change manually to make it into a 126 pole unit.

    Hi Bot team
    John is correct, the designer is not allowing the selection for 3 panel.
    when you select the unit with 480v and 3 panel you get an error at the top of the windows that said
    (Power is not supported for this main unit. Select a different load, voltage, or main unit)

    Please investigate and fix.

    We do have a Sku for the 300kva unit with 3 panel (0M-PMM300GF126 300 KVA 480V INPUT 208V OUTPUT 126 POLE)

    Mar 13, 2018 18:42:14 GMT 5.5

    Hi Reyes,
    Marques Jenkins was unable to do the change manually.
    John