1 Answers
    Jun 27, 2018 2:17:27 GMT 5.5

    The aisle bars start in wrong location on this solution: ISX0001546053-0001.

    I increased the aisle size to move the aisle bars from view so I could take a picture without the aisle bars. I made the room extra large so that some bars were always showing in the room so I would not loose them completely when I saved the solution. Now I cannot reset the aisles to the desired location. 

    Do I have to start over or can I reset something to fix this issue?

    Thanks,
    John

    Jun 28, 2018 9:52:59 GMT 5.5

    Hi John,

    I checked solution and tried on my end. Unfortunately once aisle is deleted you need to start from beginning.

    I also noticed room is custom, so please make sure you have enough space to place aisle or you'll miss aisle again.

    Best,
    Ravi.