1 Answers
    Apr 22, 2020 17:57:49 GMT 5.5

    Hi !

    If I try to configure the Easy 3M UPS system with internal batteries (or +external modular frame), the tools doesnt propose the assembly services for UPS (WASSEMSTRT-EZ-60 for 60kVA or WASSEMSTRT-EZ-120 for 80kVA and higher) and assemby services for external modular frames WASSEMEXBAT-EZ-B1

    Each time I need to add this SKU manually in add.parts....

    Can you add this services as options in addinational services window ?

    Apr 27, 2020 20:50:42 GMT 5.5

    Hi Rael,

    Thank you for reporting the issue, we are investigating the same and will get back to you.

    Thank you for your patience.

    Best Regards,
    Manjunath V.